:CRECovery:JSANalysis:OPTimize:INPut

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Command Syntax

:CRECovery{1:8}:JSANalysis:OPTimize:INPut

Where the {1:8} specifier identifies a slot number. The slot number is associated with the N1060A, N1076A/B, N1077A, N1078A, or 86108B module with Option JSA. When an 86108B module is used, the slot number is always 1.

Description

In Oscilloscope or Eye/Mask mode, optimizes a JSA spectrum that is selected to be the INPut with the :CRECovery:JSANalysis:SPECtrum command. This command sets the 86108A/B's hardware clock-recovery loop bandwidth to a minimum value which results in optimum input spectrum fidelity. If the loop can not establish lock, you can manually adjust these settings using the :CRECovery:CLBandwidth and :CRECovery:LSELect commands.

Requires FlexDCA revision A.01.70 and above.

Requires a clock-recovery module that has Option JSA (Jitter Spectrum Analysis and SW Clock Recovery Emulation).

Command Compatibility

  • N1060A Option JSA
  • 86108A/B Option JSA
  • N107X-series Option JSA

Example Command Sequence

:CRECovery{1:8}:JSANalysis:OPTimize:INPut