:CRECovery:CLBandwidth

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
FlexPLL

Command Syntax

:CRECovery{1:8}:CLBandwidth <bandwidth>

<bandwidth> is a double.

Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.

Query Syntax

:CRECovery{1:8}:CLBandwidth?

Description

Sets the loop bandwidth of the module's clock recovery PLL in Hertz. Because jitter is measured relative to the clock, jitter that is present on both the data and the recovered clock can not be detected by the DCA-X. Jitter that is within the clock recovery module's loop bandwidth appears on the recovered clock. Jitter that is outside of the loop bandwidth does not appear on the recovered clock and can be detected on the data. Selecting the loop bandwidth allows you to eliminate jitter on the recovered clock. Specify a fixed loop bandwidth using the :CRECovery <N>:LBWMode FIXed command before setting the loop bandwidth. The loop bandwidth can be any bandwidth within 30 kHz to 20 MHz specified to 3 significant digits. The default setting is 60 kHz.

To set the loop bandwidth for 83496A/B modules, use the :CRECovery{1:8}:LBANdwidth command.

Command Compatibility

  • 86108A/B
  • 83496A/B Option 300

Example Command Sequence

:CRECovery1:LBWMode FIXed
:CRECovery1:CLBandwidth 1.5E+6
:CRECovery1:RELock
*OPC?
…  //  Your code to synchronize execution timing.