:CRECovery:JSANalysis:SPECtrum:ASCii:YDATa?

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Query Syntax

:CRECovery{1:8}:JSANalysis:SPECtrum:ASCii:YDATa?

Where the {1:8} specifier identifies a slot number. The slot number is associated with the N1060A, N1076A/B, N1077A, N1078A, or 86108B module with Option JSA. When an 86108B module is used, the slot number is always 1.

Description

Returns the y-axis jitter-spectrum data in comma-separated ASCII values. The returned magnitude values are in seconds and do not require scaling. The data is sent in linear format starting from the graph's left side (lowest frequency) and progressing to the right side (highest frequency) . The frequency at any data point can be calculated as:

where,

Requires FlexDCA revision A.01.70 and above.

Requires a clock-recovery module that has Option JSA (Jitter Spectrum Analysis and SW Clock Recovery Emulation).

Command Compatibility

  • N1060A Option JSA
  • 86108A/B Option JSA
  • N107X-series Option JSA