:CRECovery:JSANalysis:SPECtrum:XORigin?

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Query Syntax

:CRECovery{1:8}:JSANalysis:SPECtrum:XORigin?

Where the {1:8} specifier identifies a slot number. The slot number is associated with the N1060A, N1076A/B, N1077A, N1078A, or 86108B module with Option JSA. When an 86108B module is used, the slot number is always 1.

Description

Returns the origin value (frequency) of the jitter spectrum data. The actual Y-formatted data can be returned as ASCII values (:CRECovery:JSANalysis:SPECtrum:ASCii:YDATa?), double values (:CRECovery:JSANalysis:SPECtrum:DOUBle:YDATa?), or float values (:CRECovery:JSANalysis:SPECtrum:FLOat:YDATa?).

The frequency at any data point can be calculated as:

where,

Requires an N1060A, N1076A, N1077A, or 86108A/B clock-recovery module that has Option JSA (Jitter Spectrum Analysis and SW Clock Recovery Emulation).

Command Compatibility

  • N1060A Option JSA
  • 86108A/B Option JSA
  • N107X-series Option JSA

Requires FlexDCA revision A.01.70 and above.

Parent Command