:DISK:SPARameter:EADifferenti
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Package License:
L-SNT
L-MFG
Command Syntax
:DISK:SPARameter:EADifferenti {ON | OFF}
Query Syntax
:DISK:SPARameter:EADifferenti?
Description
When exporting S-parameters to a Touchstone file, use this command to specify that differential S-parameters are exported. This results in a Touchstone 2.0 file. The ON argument selects differential export and the OFF argument turns off differential export.
Requires FlexDCA revision A.05.00 and above.