:DISK:SPARameter:PSET
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Package License:
L-SNT
L-MFG
Command Syntax
:DISK:SPARameter:PSET {<parameter>,<parameter>,<parameter>,… }
The <parameter> argument is an S-parameter identified using an underscore (_) character between the port numbers. For example, the S21 parameter would be sent as S2_1. Multiple S-parameters are sent as a comma-separated list.
Query Syntax
:DISK:SPARameter:PSET?
Query Response
{NONE | {<parameter>,<parameter>,<parameter>,…} }
Description
In TDR/TDT Mode, specifies a set of S-parameters to save to a Touchstone file when the :DISK:SPARamter:SAVE command is used. This is shown in the example in this topic. Any parameters sent using this command replaces any previously specified set of S-parameters; the new set does not append to the current set. A query returns the list of S-parameters. If a list has never been entered, the query returns NONE.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:DISK:SPARameter:DUT DUT1 :DISK:SPARameter:PSET S1_1, S2_1, S3_1, S4_1 :DISK:SPARameter:FNAMe "C:\Users\<user>\Documents\Keysight\FlexDCA\S-Parameter Data\SParameter_Test.s4p" :DISK:SPARameter:SAVE