:DISK:SPARameter:FWBehavior
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Package License:
L-SNT
L-MFG
Command Syntax
:DISK:SPARameter:FWBehavior {REPLace | MODify}
Query Syntax
:DISK:SPARameter:FWBehavior?
Description
Selects the file-writing behavior when saving TDR mode's S-parameter data to an existing Touchstone file. Use the :DISK:SPARameter:SAVE command to save the file.
- REPLace
- Always overwrites all S-parameters in the file. S-parameters that you are currently saving will always overwrite any S-parameters already in the file. This selection can remove S-parameter data from a file. For example, if the file already contains S21 data and you are not currently saving S21 data, the S21 data in the file will be erased.
- MODify
- Protects any existing S-parameters in the file, unless new data is available to overwrite it. S-parameters that you are currently saving will always overwrite any S-parameters already in the file.
Requires FlexDCA revision A.04.00 and above.