:DISK:SPARameter:RECall:DESTination
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Package License:
L-SNT
L-MFG
Command Syntax
:DISK:SPARameter:RECall:DESTination {SPMemory1 | SPMemory2 | SPMemory3 | SPMemory4}
Query Syntax
:DISK:SPARameter:RECall:DESTination?
Description
Selects one of four S-parameter memories to load an S-parameter file. Use the :DISK:SPARameter:RECall command to actually load the data.
The query form of the command returns the currently selected memory location.
Requires FlexDCA revision A.05.00 and above.
Example Command Sequence
:DISK:SPARameter:LFName dut_response.s2p // Select existing S-parameter file. :DISK:SPARameter:RECall:DESTination SPMemory2 // Select S-parameter memory 2. :DISK:SPARameter:RECall // Load the file data into memory 2.