:DISK:SPARameter:LFName
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Package License:
L-SNT
L-MFG
Command Syntax
:DISK:SPARameter:LFName "filename"
"filename" is a string. This command supports the DEFault common child command.
Query Syntax
:DISK:SPARameter:LFName?
Description
In TDR/TDT, Oscilloscope, or Eye/Mask modes, specifies the file (name, path, and extension) for recalling S-parameters into S-parameter memory. The default source folder is %USER_DATA_DIR%\S-Parameter Data. Use the :DISK:SPARameter:RECall command to actually load the file into memory. Use the query to determine the default S-parameter filename which is suggested based on the number of DUT ports.
| File Type | Description |
|---|---|
| .ts2 | Touchstone 2 file. Single-ended and differential data |
| .s1p | Touchstone 1 file. One-port single-ended device data (S11 or S22) |
| .s2p | Touchstone 1 file. Two-port single-ended device data (S11, S21, S22, S12) |
| .s4p | Touchstone 1 file. Four-port single-ended device data |
| .s8p | Touchstone 1 file. Eight-port single-ended device data |
| .s12p | Touchstone 1 file. Twelve-port single-ended device data |
| .s16p | Touchstone 1 file. Sixteen-port single-ended device data |
| .txt | Identical to the .s1p file type except for the .txt filename extension. |
Requires FlexDCA revision A.05.00 and above.