:DISK:WAVeform:EOSPoints

Instrument:
N1000A
DCA-M
Meas. mode:
TDR
Flex Apps:
FlexDCA

Command Syntax

:DISK:WAVeform:EOSPoints {ON | OFF | 1 | 0}

Query Syntax

:DISK:WAVeform:EOSPoints?

Query Response

 {ON | OFF | 1 | 0}

Description

Allows you to exclude off-screen data points for a displayed, active TDR step from being saved in a Y or XY formatted waveform file. Off-screen data points are always saved in internal (.wfmx format) waveform files. Off-screen data on a TDR step waveform is the leading and lagging data used to calibrate the displayed data. For additional information, refer to TDR waveform acquisition and display.

ON
Off-screen data points are not included in a saved waveform file.
OFF
Off-screen data points are saved in a waveform file. This is the default setting.

This command requires TDR Mode with an active TDR step (calibrated) displayed.

Requires FlexDCA revision A.07.80 and above.

Example Command Sequence

:ACQuire:RSPec SPERiod
:ACQuire:SPERiod:MODE MANual
:ACQuire:SPERiod 15.625e-15
:DISK:WAVeform:SAVE:FTYPe WYValues
:DISK:WAVeform:EOSPoints ON
:DISK:WAVeform:SAVE