:DISK:WAVeform:LSDigits:NUMber
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:WAVeform:LSDigits:NUMber <integer>
Where <integer> is the number of significant digits.
Query Syntax
:DISK:WAVeform:LSDigits:NUMber?
Query Response
<integer>
Description
Sets the number of significant digits for waveform amplitude and time values when saving waveform file (:DISC:WAVeform:SAVE). To turn on or off significant digit limiting, use the :DISK:WAVeform:LSDigits parent command. The default value is 6 significant digits. The minimum value is 1. The maximum value is 14.
Requires FlexDCA revision A.05.70 and above.