:DISK:WAVeform:FNAMe:USTandard
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:WAVeform:FNAMe:USTandard
Description
Resets the file name for the waveform file from using a custom name to using the standard name in the following form:
Waveform_<date><autonumber>.<extension>
For example, Waveform_2020-10-23_1.wfmx. Refer to :DISK:WAVeform:FNAMe to learn about standard and custom names.
Requires FlexDCA revision A.05.70 and above.