:DISK:WAVeform:SAVE:VSA:QSOUrce
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:WAVeform:SAVE:VSA:QSOUrce {CHANnel{N} | DIFF{1:4} | FUNCtion{1:16} | WMEMory{1:8} | TRACe{1:128}}
Where N identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, CHANnel3C.
Query Syntax
:DISK:WAVeform:SAVE:VSA:QSOUrce?
Query Response
{CHAN{N} | DIFF{1:4} | FUNC{1:16} | WMEM{1:8} | TRAC{1:128}}
Description
In Oscilloscope and Eye Mask modes, selects a second signal source for a VSA Waveform Recording file when the COMPlex data is selected using the :DISK:WAVeform:SAVE:VSA_DTYPe command. Use the :DISC:WAVeform:SAVE command to actually save the file.
Requires FlexDCA revision A.05.70 and above.