:DISK:WAVeform:LINTerpolate
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:WAVeform:LINTerpolate {ON | OFF | 1 | 0}
Query Syntax
:DISK:WAVeform:LINTerpolate?
Query Response
{ON | OFF | 1 | 0}
Description
Turns on linear interpolation to make the Y-values equally spaced in the saved waveform file. Linear interpolation is available for the following data formats as selected with the :DISK:WAVeform:SAVE:FTYPe command:
- Waveform Files, Y values (WYValues)
- Waveform Files, XY values (WXYValues)
- Pattern Waveform, comma delimited (WPATtern)
- VSA Recording, tab delimited (VSATsv)
- VSA Recording, comma delimited (VSACsv)
Requires FlexDCA revision A.05.70 and above.