:DISK:WAVeform:LSDigits
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:WAVeform:LSDigits {ON | OFF | 1 | 0}
Query Syntax
:DISK:WAVeform:LSDigits?
Query Response
{ON | OFF | 1 | 0}
Description
When saving waveforms to a file (:DISC:WAVeform:SAVE), turns on or off the limiting of waveform data values (x or y) to the number of significant digits specified with the :DISK:LSDigits:NUMber child command. The default setting is OFF. Significant digit limiting applies to the following waveform file types:
-
Internal pattern waveforms
Y-value waveforms
XY-value waveforms
Pattern waveforms
VSA waveforms
This command does not apply to internal format waveform files.
Requires FlexDCA revision A.05.70 and above.
Child Commands
:NUMbersets the number of significant digits to use.