:DISPlay:WINDow:LLTResults:TWDouble
Command Syntax
:DISPlay:WINDow:LLTResults:TWDouble {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:WINDow:LLTResults:TWDouble?
Query Response
{1 | 0}
Description
When the Limit Lines results panel is displayed below the waveform window, use this command to specify the width of the Limit Lines results panel. The panel can have the same width as the waveform window (ON) or half the width (OFF).Use the :DISPlay:WINDow:LLTResults:LOCation command to align the panel with either the left or right edge of the waveform window.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:LLTResults:TWDouble OFF :DISPlay:WINDow:LLTResults:LOCation RSECondary :DISPlay:TSMode HSIZe