:DISPlay:WINDow:OJITter:LOCation

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter

Command Syntax

:DISPlay:WINDow:OJITter:LOCation {PRIMary | LSECondary | RSECondary | FTABs}

Query Syntax

:DISPlay:WINDow:OJITter:LOCation?

Query Response

{PRIM | LSEC | RSEC | FTAB}

Description

Selects the location to display the Output Jitter results panel for PAM4 signals. Use the arguments listed below to specify the position.

PRIMary
The panel is placed in the large area normally reserved to display the waveforms.
LSECondary
The panel is left aligned beneath the displayed waveform. Use the :DISPlay:WINDow:OJITter:TWDouble command to select whether the panel covers the full display width or is half the width. Since the panel is normally hidden after sending this argument, send the :DISPlay:TSMode command to expand (show) the panel.
RSECondary
The panel is right aligned beneath the displayed waveform. Use the :DISPlay:WINDow:OJITter:TWDouble command to select whether the panel covers the full display width or is half the width. Since the panel is normally hidden after sending this argument, send the :DISPlay:TSMode command to expand (show) the panel.
FTABs
The panel is undocked (floated) from FlexDCA's window. To re-dock the panel, resend the command using the PRIMary, LSECondary, or RSECondary arguments.

Requires FlexDCA revision A.06.50 and above.

Example Command Sequence

:DISPlay:WINDow:OJITter:TWDouble OFF
:DISPlay:WINDow:OJITter:LOCation RSECondary
:DISPlay:TSMode HSIZe

Sibling Commands