:DISPlay:WINDow:JITTer:LOCation
Jitter
NRZ
Command Syntax
:DISPlay:WINDow:JITTer:LOCation {PRIMary | LSECondary | RSECondary | FTABs}
Query Syntax
:DISPlay:WINDow:JITTer:LOCation?
Query Response
{PRIM | LSEC | RSEC | FTAB}
Description
Selects the location to display the Jitter results panel for NRZ signals. Use the arguments listed below to specify the position.
- PRIMary
- The panel is placed in the large area normally reserved to display the waveforms.
- LSECondary
- The panel is left aligned beneath the displayed waveform. Use the
:DISPlay:WINDow:JITTer:TWDoublecommand to select whether the panel covers the full display width or is half the width. Since the panel is normally hidden after sending this argument, send the:DISPlay:TSModecommand to expand (show) the panel. - RSECondary
- The panel is right aligned beneath the displayed waveform. Use the
:DISPlay:WINDow:JITTer:TWDoublecommand to select whether the panel covers the full display width or is half the width. Since the panel is normally hidden after sending this argument, send the:DISPlay:TSModecommand to expand (show) the panel. - FTABs
- The panel is undocked (floated) from FlexDCA's window. To re-dock the panel, resend the command using the
PRIMary,LSECondary, orRSECondaryarguments.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:JITTer:TWDouble OFF :DISPlay:WINDow:JITTer:LOCation RSECondary :DISPlay:TSMode HSIZe