:DISPlay:WINDow:JGRaphs:TWDouble
Jitter
Command Syntax
:DISPlay:WINDow:JGRaphs:TWDouble {ON | OFF}
Query Syntax
:DISPlay:WINDow:JGRaphs:TWDouble?
Query Response
{1 | 0}
Description
When the Graphs window is displayed, use this command to specify the width of the Graphs window. The window can have the same width as the waveform window (ON) or half the width (OFF).Use the :DISPlay:WINDow:JGRaphs:LOCation command to align the panel with either the left or right edge of the waveform window.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:JGRaphs:TWDouble OFF :DISPlay:WINDow:JGRaphs:LOCation RSECondary :DISPlay:TSMode HSIZe