:DISPlay:WINDow:JGRaphs:LOCation
Jitter
Command Syntax
:DISPlay:WINDow:JGRaphs:LOCation {PRIMary | LSECondary | RSECondary | FTABs}
Query Syntax
:DISPlay:WINDow:JGRaphs:LOCation?
Query Response
{PRIM | LSEC | RSEC | FTAB}
Description
Selects the location to display the Graphs window. Use the arguments listed below to specify the position.
- PRIMary
- The window is placed in the large area normally reserved to display the waveforms.
- LSECondary
- The window is left aligned beneath the displayed waveform. Use the
:DISPlay:WINDow:JGRaphs:TWDoublecommand to select whether the window covers the full display width or is half the width. If the window is hidden after sending this argument, send the:DISPlay:TSModecommand to expand (show) the window. - RSECondary
- The window is right aligned beneath the displayed waveform. Use the
:DISPlay:WINDow:JGRaphs:TWDoublecommand to select whether the window covers the full display width or is half the width. If the window is hidden after sending this argument, send the:DISPlay:TSModecommand to expand (show) the panel. - FTABs
- The window is undocked (floated) from FlexDCA's window. To re-dock the window, resend the command using the
PRIMary,LSECondary, orRSECondaryarguments.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:JGRaphs:TWDouble OFF :DISPlay:WINDow:JGRaphs:LOCation RSECondary :DISPlay:TSMode HSIZe