:DISPlay:WINDow:OJITter:TWDouble
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter
Command Syntax
:DISPlay:WINDow:OJITter:TWDouble {ON | OFF}
Query Syntax
:DISPlay:WINDow:OJITter:TWDouble?
Query Response
{1 | 0}
Description
When the Output Jitter measurement results panel is displayed (PAM4 signals) below the waveform window, use this command to specify the width of the Output Jitter panel. The panel can have the same width as the waveform window (ON) or half the width (OFF).Use the :DISPlay:WINDow:OJITter:LOCation command to align the panel with either the left or right edge of the waveform window.
Requires FlexDCA revision A.06.50 and above.
Example Command Sequence
:DISPlay:WINDow:OJITter:TWDouble OFF :DISPlay:WINDow:OJITter:LOCation RSECondary :DISPlay:TSMode HSIZe