:EMEMory:DSTatus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:DSTatus?
Where the required specifier {1:8} identifies one of eight eye memories.
Query Response
{CORR | INV}
Description
Returns the status of the specified waveform memory. Up to eight memories are available. To query the reason for the current state of the memory, use the :EMEMory:DSTatus:REASon? query. The following responses can be returned:
CORR- The eye memory location contains eye waveform data. To clear memory, use the
:EMEMory:CLEarcommand. INV- The eye memory location does not contain waveform data.
Requires FlexDCA revision A.05.70 and above.
Example Command
:EMEMory3:DSTatus?