:EMEMory:UNAMe
Command Syntax
:EMEMory{1:8}:UNAMe <string>
Where the required specifier {1:8} identifies one of eight eye memories.
Where "string" is a custom name for a memory waveform.
Requires FlexDCA revision A.03.00 and above.
Query Syntax
:EMEMory{1:8}:UNAMe?
Description
Assigns a custom user name to an eye-memory waveform. User names are helpful because they identify what a waveform represents rather than the oscilloscope's input channel. For example, you could assign user name "DUT Output" to the memory 2 waveform. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string. To assign the user name to the name of the gray-scale and color-grade database waveform file that was imported into eye memory, use the :EMEMory:UNAMe:UFName command.
Custom user names can by created for other waveforms using the following commands:
:CHANnel:UNAMe:CMODe:UNAMe:DIFF:UNAMe:FUNCtion:UNAMe:TDR:DUT:DIFFerential:NPORt:UNAMe:TDR:DUT:DIFFerential:PPORt:UNAMe:TDR:DUT:DIFFerential:SIGNal:UNAMe:TRACe:UNAMe:WMEMory:UNAMe
Example Command Sequence
:EMEMory2:UNAMe "DUT Output"