:EMEMory:DSTatus:REASon?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:DSTatus:REASon?
Where the required specifier {1:8} identifies one of eight eye memories.
Query Response
<string>
Description
Returns a description of the status of the specified eye memory. If an eye waveform is currently in the specified eye memory location, the name of the source waveform will be returned. For example, "Source: Channel 1A". If the eye memory is empty, the string "Please select a file." is returned. If the file is corrupt or an incorrect type, the string "Unable to load file." is returned. To check the status of the eye memory, use the :EMEMory:DSTatus? parent query.
Requires FlexDCA revision A.05.70 and above.
Example Command
:EMEMory3:DSTatus:REASon?