:EMEMory:STATus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Query Syntax
:EMEMory{1:8}:STATus?
Where the required specifier {1:8} identifies one of eight eye memories.
Query Response
{AVA | UNAV}
Description
Queries the availability of eye memory for use. Eye memory becomes available (AVA) after data has been loaded into memory using the :EMEMory:FILE:LOAD command. Eye memory does not need to be displayed to be classed as available. Eye memory is unavailable (UNAV) if data has not been loaded into the memory.
Use the :EMEMory:DISPlay command query to determine if a Eye memory waveform is displayed.
Example Command
:EMEMory3:STATus?