:EMEMory:UNAMe:UFName
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:UNAMe:UFName
Where the required specifier {1:8} identifies one of eight eye memories.
Description
Automatically sets the eye memory's user name to the name of the waveform's source file. If the waveform was loaded from a displayed input channel, the name of the file that was automatically created when the data was loaded is used. To learn about user names, use the default user name, or enter a custom user name, use the :EMEMory:UNAMe command.
Requires FlexDCA revision A.05.70 and above.
Example Command Sequence
:EMEMory2:UNAMe:UFName