:EMEMory:COLor
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Command Syntax
:EMEMory{1:8}:COLor {TCOLor1 | TCOLor2 | … | TCOLor16}
Where the required specifier {1:8} identifies one of eight eye memories.
Query Syntax
:EMEMory{1:8}:COLor?
Description
Selects the color used to identify a channel on the screen. Waveform color assignments are saved as part of an instrument Setup file (:DISK:SETup:SAVe). Waveform colors are reset to their default values by a default setup (:SYSTem:DEFault) or factory preset (:SYSTem:FACTory).
| Color | Argument | Color | Argument | Color | Argument | Color | Argument | |||
|---|---|---|---|---|---|---|---|---|---|---|
| TCOLor1 | TCOLor2 | TCOLor3 | TCOLor4 | |||||||
| TCOLor5 | TCOLor6 | TCOLor7 | TCOLor8 | |||||||
| TCOLor9 | TCOLor10 | TCOLor11 | TCOLor12 | |||||||
| TCOLor13 | TCOLor14 | TCOLor15 | TCOLor16 |
To change the color of any waveform, use the following additional subsystem :COLor commands:
| Command | Description |
|---|---|
:CHANnel:COLor
|
Sets color of channel waveforms. |
:CMODe:COLor
|
Sets color of common-mode waveforms. |
:DIFF:COLor
|
Sets color of differential waveforms. |
:EMEMory:COLor
|
Sets color of eye memory waveforms |
:FUNCtion:COLor
|
Sets color of math function output waveforms. |
:TRACe:COLor
|
Sets color of T-domain parameter or S-parameter waveforms in TDR/TDT mode. |
:WMEMory:COLor
|
Sets color of waveform memories. |
Requires FlexDCA revision A.04.50 for colors 13 through 16.
Example Command
:EMEMory3:COLor TCOLor1