:EMODules:SIMulator:SRATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:EMODules:SIMulator:SRATe {LOW | STANdard | HIGH}
Query Syntax
:EMODules:SIMulator:SRATe?
Description
Selects the waveform simulation rate which affects the amount of CPU usage devoted to data simulation: LOW, STANdard, or HIGH. The default setting is STANdard. Adjusting this setting can affect the performance of FlexDCA and any concurrently running applications.
Requires FlexDCA revision A.02.00 and above.
Example Command
:EMODules:SIMulator:SRATe STANdard