:EMODules:SLOT:SELection

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:SLOT{1:8}:SELection {EMPTy | DCA | DCAM | RTSCope | AWGenerator | SWITch | DEMini | DOMini | OEMini | QEMini}

Where the {1:8} specifier identifies a specific module by slot.

Query Syntax

:EMODules:SLOT{1:8}:SELection?

Query Response

{EMPT | DCA | DCAM | RTSC | AWG | SWIT | DEM | DOM | OEM | QEM}

Description

Assigns an extended module to an internal slot (1-4) or simulated slot (5-8). The DCA argument assigns an N1000A to slot 1 (the N1000A occupies slots 1 through 4). A N1000A can not be assigned to slots 5 through 8. The AWGenerator is the only argument that is available when running FlexDCA in FlexRT.

Supported optical switches are used by the FlexOTO application and not by FlexDCA. However, FlexDCA's ability to connect an optical switch is provided so that you can control an optical switch from FlexDCA or exercise an switch outside of FlexOTO for troubleshooting purposes. FlexOTO does not provide or allow direct switch control by users or via remote SCPI commands. After connecting to an optical switch, you can control the switch using commands in the :FRAMe subsystem and :SLOT subsystem.

Extended modules can be simulated modules, a DCA-M (such as the N1090A DCA-M is a single optical channel sampling oscilloscope), an M8194/5/6A Arbitrary Waveform Generator (AWG), or an optical switch. If you install an arbitrary waveform generator or a simulated module, use the commands in the :SOURce subsystem to configure the module's waveform. For an AWG, additional commands are available in the :EMODules subsystem.

Use the command query to determine what, if any, extended module is assigned to each slot.

Argument Availability
Argument Assigns N1010A FlexDCA N1010A FlexDCA
(in FlexRT)
N1000A
Slots 1-4 Slots 5-8 Slots 1-4 Slots 5-8 Slots 1-4 Slots 5-8
EMPTy Clears (removes) an assigned module ♦ ♦       ♦
DCA Assigns a N1000A to slots 1 through 4 ♦       ♦  
DCAM Assigns an N109x-series or N107x-series DCA-M module ♦ ♦       ♦
RTSCope Assigns a Keysight UXR-series oscilloscope to slots 1 through 4.     ♦      
AWGenerator Assigns a Keysight M8194/5/6A arbitrary waveform generator to a slot. ♦ ♦   ♦   ♦
SWITch Assigns an optical switch ♦ ♦       ♦
DEMini Assigns simulated dual-electrical module ♦ ♦       ♦
DOMini Assigns simulated dual-optical module ♦ ♦       ♦
OEMini Assigns simulated electrical-optical module ♦ ♦       ♦
QEMini Assigns simulated quad-electrical module ♦ ♦       ♦

Requires FlexDCA revision A.06.00 for the M8195A and M8196A. Optical switch support requires revision A.07.00. For other extended modules, requires FlexDCA revision A.02.00 and above.

Example Command Sequence

:EMODules:SLOT1:SELection QEMini EMPTy /* Remove DCA internal slots from slots 1 through 4 */
:EMODules:SLOT2:SELection QEMini /* Assign simulated quad-electrical to slot 2 */