:EMODules:SLOT:CMEThod?
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:EMODules:SLOT{1:8}:CMEThod?
Where the {1:8} specifier identifies a specific module by slot.
Query Response
{USB | LOC | NONE}
Description
Use this query to determine if an extended module is connected to FlexDCA. As the only connection method for a DCA-M module is via USB, the value returned can be USB or NONE. The returned strings are:
USB- Indicates a DCA-M module is connected.
LOC- Indicates an optical switch is connected.
NONE- There no module in the slot.
Requires FlexDCA revision A.05.00 and above.
Example Command
:EMODules:SLOT4:CMEThod?