:JSAMemory:JSANalysis:SPECtrum:PEAKs?
Instrument:
                                                N1000A
                                                N109x
                                                UXR Scope
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Meas. mode:
                                                Scope
                                                Eye
                                                Jitter
                                            Waveform type:
                                                NRZ
                                                PAM4
                                            Package License:
                                                L-RND
                                                L-SNT
                                            Query Syntax
:JSAMemory:JSANalysis:SPECtrum:PEAKs?
Description
Returns an ASCII comma-delimited listing of the spectrum peaks (frequency and magnitude values) shown on the Spectrum Peaks table. This table is shown in the following picture. These peaks are also identified and shown on the Jitter Spectrum graph within the band limiting markers. The peak values are returned in order from the lowest to the highest frequency, regardless of their order shown in the Spectrum Peaks table. The returned value pairs are returned in the following order:
<frequency>,<magnitude>,<frequency>,<magnitude>,<frequency>,<magnitude>,…
                                                 
                                            
                                                 
                                            
Requires FlexDCA revision A.04.00 and above.