:JSAMemory:MEASured:SSTatus
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:MEASured:SSTatus {AVAilable | UNAVailable}
Query Syntax
:JSAMemory:MEASured:SSTatus?
Description
Enables or disables the selection of the Measured reference clock signal for jitter spectrum analysis. Once enabled, use the :JSAMemory:SPECtrum command to select the Measured spectrum type.
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, L-RND package license (includes feature F-JIT Enhanced Jitter Analysis) is required.
Requires FlexDCA revision A.02.50 and above.