:JSAMemory:JSANalysis:SPECtrum:XORigin?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Query Syntax
:JSAMemory:JSANalysis:SPECtrum:XORigin?
Description
Returns the frequency origin of the JSA spectrum data. Use this value along with the values returned by the :XINCrement and :POINts sibling queries to determine the frequency of any point returned as :ASCii:YDAta, :DOUBle:YDATa, or FLOat:YDATa.
Requires FlexDCA revision A.04.00 and above.