:JSAMemory:JSANalysis:SPECtrum:PEAKs:ALL?
Instrument:
                                                N1000A
                                                N109x
                                                UXR Scope
                                            Flex Apps:
                                                FlexDCA
                                                FlexRT
                                            Meas. mode:
                                                Scope
                                                Eye
                                                Jitter
                                            Waveform type:
                                                NRZ
                                                PAM4
                                            Package License:
                                                L-RND
                                                L-SNT
                                            Query Syntax
:JSAMemory:JSANalysis:SPECtrum:PEAKs:ALL?
Description
Returns an ASCII comma-delimited listing of all of the spectrum peaks (frequency and magnitude values) shown on the Jitter Spectrum graph, without regard to the band limiting markers. The peak values are returned in order from the lowest to the highest frequency in the following order:
<frequency>,<magnitude>,<frequency>,<magnitude>,<frequency>,<magnitude>,…
                                                 
                                            
Requires FlexDCA revision A.04.00 and above.