:LTESt:MEASure:SWAVeform:FUNCtion:FNAMe
Command Syntax
:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:FNAMe "<path substitution string>\subfolder\filename"
Where {1:64} identifies a function.
Where <path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
Where "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\Waveforms.
Where "filename" is a string without the filename extension.
Query Syntax
:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:FNAMe?
Description
Specifies the file name (including path and file name extension) for saving a function waveform (.wfmx) reporting file for an measurement limit test. Use the :LTESt:MEASure:SWAVeform:FUNCtion{1:64}:STATe command to enable and disable waveform reporting for the channel. This command supports the DEFault common child command.
Do not include an extension when specifying the filename.
The default folder for storing function waveform files is in %USER_DATA_DIR%\Waveforms as shown in this pictures. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Waveforms\filename.
File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Preset.
Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.
Example Command
:LTESt:MEASure:SWAVeform:FUNCtion4:FNAMe "DUT132"