:LTESt:MEASure:SWAVeform:CMODe:WMEMory
Instrument:
N1010A
N1000A
Meas. mode:
TDR
Flex Apps:
FlexDCA
This command is compatible with TDR/TDT mode only.
Command Syntax
:LTESt:MEASure:SWAVeform:CMODe{1:8}{A|C}:WMEMory WMEMory{1:8}
Where the specifier {1:8}{A|C} identifies a common-mode channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:MEASure:SWAVeform:CMODe{1:8}{A|C}:WMEMory?
Description
Upon completion of an measurement limit test, selects a waveform memory as a destination to save a common-mode waveform. Use the :LTESt:MEASure:SWAVeform:CMODe:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test
Requires FlexDCA revision A.04.00 and above.
Example
:LTESt:MEASure:SWAVeform:CMODe2A:WMEMory WMEMory3