:LTESt:MEASure:SWAVeform:DIFF:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SWAVeform:DIFF{1:8}{A|C}:WMEMory WMEMory{1:8}
Where {1:8}{A|C} identifies a differential channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:MEASure:SWAVeform:DIFF{1:8}{A|C}:WMEMory?
Description
Upon completion of an measurement limit test, selects a waveform memory as a destination to save a differential waveform. Use the :LTESt:MEASure:SWAVeform:DIFF:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test
Example
:LTESt:MEASure:SWAVeform:DIFF2A:WMEMory WMEMory3