:LTESt:MEASure:SWAVeform:CHANnel:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory WMEMory{1:8}
CHANnel{1:8}{A|B|C|D} <N> identifies the channel as in CHANnel1A, CHANnel1B, …, CHANnel4D.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:MEASure:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory?
Description
Upon completion of an measurement limit test, selects a waveform memory as a destination to save a channel waveform. Use the :LTESt:MEASure:SWAVeform:CHANnel:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test.