:LTESt:MEASure:SWAVeform:FUNCtion:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:WMEMory WMEMory{1:8}
Where {1:64} identifies a function.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:MEASure:SWAVeform:FUNCtion{1:64}:WMEMory?
Description
Upon completion of an measurement limit test, selects a waveform memory as a destination to save a function waveform. Use the :LTESt:MEASure:SWAVeform:FUNCtion:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test.
Example
:LTESt:MEASure:SWAVeform:FUNCtion2:WMEMory WMEMory3