:LTESt:MEASure:SWAVeform:CHANnel:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SWAVeform:CHANnel{1:8}{A|B|C|D}:STATe {DISK | MEMory | OFF}
Where the specifier {1:8}{A|B|C|D} identifies the channel.
Query Syntax
:LTESt:MEASure:SWAVeform:CHANnel{1:8}{A|B|C|D}:STATe?
Query Response
{DISK | MEM | OFF}
Description
Saves a channel waveform to a file or memory location after the measurement limit test acquires the specified number of failures. Use the :LTESt:MEASure:MLIMit:FAILures command to enter the number of failures to limit the test. The following command arguments are available:
- DISK
- Saves the waveform to a file. Use the
:LTESt:MEASure:SWAVeform:CHANnel:FNAMecommand to specify the file name. - MEMory
- Saves the waveform to a memory location. Use the
:LTESt:MEASure:SWAVeform:CHANnel:WMEMorycommand to specify the memory location. - OFF
- Turns off the saving of a common-mode waveform.