:MEASure:JITTer:POJitter:JHNU:LOCation?
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Meas. panel:
Timing Jitter
Timing Jitter
Query Syntax
:MEASure:JITTer:POJitter:JHNU:LOCation?
Query Response
"<row location>"
For example, 2.
Description
Returns an index string that identifies the measurement cell of the :MEASure:JITTer:POJitter:JHNU measurement results in the Timing Jitter panel. If the measurement is not listed in the table, a "−1" is returned.
Requires FlexDCA revision A.08.30 and above.