:MTESt:ALIGnment:X
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:ALIGnment:X {AUTomatic | MANual}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:ALIGnment:X?
Description
Selects automatic or manual horizontal alignment of the selected mask to the eye diagram. If MANual is selected, use the following commands to scale the mask:
Requires FlexDCA revision A.03.00 and above.