:MTESt:AOPTimize
Command Syntax
:MTESt{1:16}:AOPTimize {ON | OFF | 1 | 0}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:AOPTimize?
Query Response
{1 | 0}
Description
Enables or disables optimization of the placement of the center mask region during mask alignment. Mask are automatically aligned whenever they are loaded using the :MTESt:LOAD command. When optimization is turned on, the center region (Region 1) is offset along the X-axis to achieve the best mask test margin when mask alignment is performed. The amount of offset is in the range of ±25% of the unit interval. By default, optimization is off. When designing masks, optimization may be defined in a specific mask file by embedding the MaskAlignmentOptimize element in the setup block at the end of the mask file.
Not all mask test standards allow optimization. Optimization is enabled in mask files provided by Keysight Technologies as allowed by relevant standards. To ensure conformance, consult appropriate standards documents before enabling optimization.