:MTESt:ALIGnment:Y:METHod
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:ALIGnment:Y:METHod {DISPlay | EWINdow}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:ALIGnment:Y:METHod?
Description
Specifies the method used to align the mask's Y-axis. It ensures that the mask will be properly adjusted on the display. Alignment mode needs to be specified for optical NRZ masks. Use the :MTESt:ALIGnment:Y command to select automatic or manual mask scaling.
DISPlay- Aligns the mask's Y axis using the Vbase and Vtop of the eye diagram. This can be used for all mask tests.
EWINdow- Align the Y axis to the eye boundaries (one and zero logic levels). This argument applies to optical NRZ mask. It is typically used to align 10 GB Ethernet masks. This alignment mode does not apply to fixed-voltage masks. Use
:MEASure:EBOundary:LEFTand:MEASure:EBOundary:RIGHtto set the eye boundaries.
Requires FlexDCA revision A.03.00 and above.