:MTESt:YTRack
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MTESt{1:16}:YTRack {ON | OFF | 1 | 0}
Where the {1:16} specifier identifies a specific mask.
Query Syntax
:MTESt{1:16}:YTRack?
Query Response
{1 | 0}
Description
Turns logic-level tracking on or off, which affects the masks Y-axis scaling and position. Use the :MTESt:Y2 command to adjust logic-level one. Use the :MTESt:Y1 command to adjust logic-level zero. Changing a logic-level from the default value specified in the mask sets the mask scale mode selection to X-axis only (:MTESt:SMODe XONLy).
- ON
- Logic level tracking is enabled and the logic levels track each other, allowing you to manually move the mask up and down on the display. For example, if you adjust the logic 1 level by 5 mW, the logic 0 level will also move by 5 mW.
- OFF
- You can independently scale the mask to logic level one and zero.