:PTIMebase:RFRequency
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Module:
N1060A
Command Syntax
:PTIMebase{1 | 2}:RFRequency <frequency>
Where the {1 | 2} specifier identifies module slot number that is associated with N1060A.
Where <frequency> is a double.
Query Syntax
:PTIMebase{1 | 2}:RFRequency?
Description
Specifies the frequency of the reference clock at the input of the N1060A module. You must first select an external reference source using the :PTIMebase:RSOurce command.
As of FlexDCA revision A.08.30 and above, this command no longer supports the 86107A precision timebase or 86108A/B precision waveform analyzer modules.