:PTIMebase:RSOurce
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Module:
N1060A
Command Syntax
:PTIMebase{1 | 2}:RSOurce {INTernal | EXTernal}
Where the {1 | 2} specifier identifies module slot number that is associated with N1060A.
Query Syntax
:PTIMebase{1:8}:RSOurce?
Description
This N1060A command selects an internal or external reference source for the precision timebase. When an external source is selected, use the :PTIMebase:RFRequency command to specify the frequency of the input reference signal.