:PTIMebase:RTReference
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Module:
N1060A
Command Syntax
:PTIMebase{1 | 2}:RTReference
Where the {1 | 2} specifier identifies module slot number that is associated with N1060A.
Description
Resets the time reference. If the time reference fails to set, an error is produced. The usual causes for not being able to set the time reference include missing, too small, or too large signal or a frequency that is not in the specified ranges.
Use of an *OPC? query to pause program execution while waiting for this command to execute.
As of FlexDCA revision A.08.30 and above, this command no longer supports the 86107A precision timebase or 86108A/B precision waveform analyzer modules.