:PTIMebase:VPTBsignals

Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Module:
N1060A

Command Syntax

:PTIMebase{1 | 2}:VPTBsignals {ON | OFF | 1 | 0}

Where the {1 | 2} specifier identifies module slot number that is associated with N1060A.

Query Syntax

:PTIMebase{1 | 2}:VPTBsignals?

Description

Turns on and off the display of the two precision timebase IQ input waveforms. These two waveforms are displayed on the Precision Timebase tab, which is located on Setup dialogs for N1060A modules. To return the waveforms to the computer, use the :WAVeform:SOURce command. The query form of the command returns the current display state, on or off.

As of FlexDCA revision A.08.30 and above, this command no longer supports the 86107A precision timebase or 86108A/B precision waveform analyzer modules.

Requires FlexDCA revision A.05.30 and above.