:TDR:DEEMbed:DUT:PORT:FIXTure
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DEEMbed:DUTN:PORTM:FIXTure {NONE | FCOMF}
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Where M indicates one of 16 possible DUT ports. For example, :PORT3.
Where F identifies a specific fixture component. There can be up to sixteen fixture components identified by letters A through P. For example, FCOMA.
Query Syntax
:TDR:DEEMbed:DUTN:PORT{1:16}:FIXTure?
Description
Associates (or disassociates) a fixture component with the specified DUT port. Components are named FCOMA through FCOMP. Once a component is selected, use the :DPORt and :TPORt child commands to define how the fixture is connected to the DUT. Refer to the :TDR:DEEMbed:DUT:ENABle command for more information.
Requires FlexDCA revision A.05.30 and above.